Get Started with RealSense ID. Facial authentication solution.

Congratulations! Now that you’ve got your RealSense ID device, start using it by following these simple steps.

What’s in the box?

Connecting RealSense ID

Illustration showing the F455 camera being connected to a laptop with USB C cable

Using the provided USB 2 Type C cable, connect the peripheral to your PC or host device.

Activate your Device(s)

The F45x cameras are pre-installed with the facial authentication and anti-spoofing software.
There is no need for a separate SW purchase, registration, or activation.

By using the facial authentication and anti-spoofing software,  you are agreeing to the Terms and Conditions of the End-User License Agreement.

Get the latest RealSense ID SDK

The RealSense ID SDK includes the RealSense ID API, documentation, viewer application, and useful tools, as well as code samples for Windows and Linux.​
It can be found on the RealSense GitHub page.​

Download the source code or check out our repo. Follow the build instructions to build our host library and tools.

Using the RealSense ID Viewer software

The viewer software is designed to allow you to quickly test and evaluate a variety of features of your new RealSense ID device.

Enroll a new user

After entering your name, the system will enroll you and display a success message.

Sit or stand about 20 inches (50 cm) from the camera, ideally with good ambient light and minimal backlighting. Select Enroll and enter your name.

Follow the instructions on the screen to turn your head.

Select the pictures icon next to the Enroll button. Add the user’s name, then select a picture to upload to use for enrollment purpose only.


Authentication

Once you have enrolled, you can test authentication

Select Authenticate to authenticate you once. With the repeat button (double arrows next to Authenticate), the system will continuously attempt to authenticate you until you select Stop.

rsid-viewer, configuration, facial authentication

Deleting a user

Delete users by selecting the checkboxes next to their names, and then select the trash icon to delete them. This action cannot be undone – any users accidentally deleted must be re-enrolled. The top checkbox can be used to delete all enrolled users.

rsid-viewer, configuration, facial authentication

Settings

There are a number of configurable settings that allow you to customize the operation of your F450/F455.

Using the gear icon in the top right corner will open Settings.

rsid-viewer, configuration, facial authentication

Face Selection – If Single is selected, the device will return results only for one face, which is the best candidate found. When Multi is selected, the device will return results for all the faces detected in the frame.​ This is a small latency and power impact when running Multi as the pipeline is run on all the faces in the image.

Host Mode – By default, the user database information is saved on the F450/F455 device. By selecting Enabled, the user database information can be saved in another location.​

Preview Format – Select which format to show for previews.​

Dump Mode – Enabled turns on frame dumps but disables live preview. Frame dumps are located in a subfolder called dumps.

Security Level – This setting enables the ability to test an operating mode that supports partially covered faces (e.g. due to face masks). Medium confidence will allow authentication with greater tolerance, where High confidence might reject partially covered faces in some situations.​

Operation Mode – This setting allows you to choose what features you wish to enable on the device.​

  • All runs all functionality for facial authentication including facial recognition and anti-spoofing of enrolled users. This mode offers the highest level of facial authentication.
  • Detect runs only facial detection, not anti-spoofing, facial authentication, or facial recognition, regardless of whether or not the person is an enrolled user.
  • Spoof runs anti-spoofing only, a method that distinguishes between genuine and fake faces.
  • Recog runs facial recognition of enrolled users without anti-spoofing. This is not as secure as facial authentication that is performed in the All operation mode.

Camera Rotation – In situations where the camera needs to be rotated (for example, mounted upside down to conform to a specific industrial design), the operational mode should be set to visually correct the rotation.​

Firmware Update – Selecting Browse will enable updating the firmware on the connected device as described in the following section.

Updating Firmware

You can download the latest firmware here.

F45x devices running firmware 5.7.0.301 or newer require a license for facial recognition and spoofing features to work.

When needed, you will be prompted to update the firmware before using.

First download the latest firmware here. Then go to Settings (Gear icon) and select Browse next to Firmware update.

Make sure your device is securely connected and navigate to the firmware file you just downloaded.

Open the file and wait for the update to complete. When the update is completed, the device will reboot and reconnect with this application.​

Documentation

We have created a documentation portal to help you get started. For additional information please refer to the RealSense ID Solution documentation page.

Receive updates about the latest news on facial authentication solutions.

Top
Contact Sales
Server Region: North America | Hostname: ip-172-16-1-22